The adrv9026_top_no_fill_config1.bsdl file should be used for systems that operate with the Tx/Rx SYNC pins in LVDS mode and include the JESD pins as part of boundary scan.

The adrv9026_top_no_fill_config1_nojesd.bsdl file should be used for systems that operate with the Tx/Rx SYNC pins in LVDS mode without the JESD pins as part of boundary scan.

The adrv9026_top_no_fill_config2.bsdl file should be used for systems that operate with the Tx/Rx SYNC pins in CMOS mode and include the JESD pins as part of boundary scan.

The adrv9026_top_no_fill_config2_nojesd.bsdl file should be used for systems that operate with the Tx/Rx SYNC pins in CMOS mode without the JESD pins as part of boundary scan.